Full control and full automation

Overview_TEXT

Tổng quan

BOT Elektrownia Opole S.A. power plant is located 9 kilometres north from the city of Opole, downstream of the Mala Panew River which flows into the Odra River. The existing and planned production facilities cover approximately 290 hectares. This location ensures good opportunities for providing the power supply to the South-Western area of Poland as well as the transfer of energy to other parts of the country and abroad.

At present, BOT Elektrownia Opole S.A. power plant runs four hard-coal fired energy power generating units (of the six planned originally). The Opole power plant was the last significant investment of the Polish power engineering industry. Its generating units were commissioned during the years 1993-1997. As the construction of the generating units progressed, the Opole power plant was equipped with the environment protection equipment and now meets all national and EU environment legislation and does not need to spend significant money to keep pace with tightening engine-emission standards.

Equipped with four generating blocks, BOT Elektrownia Opole S.A. is the most modern hard coal fuelled power station in Poland. The overall installed capacity is equal to 1492 MW (1x376 MW; 1x373 MW; 1x373 MW; 1x370 MW) and achieved capacity reaches 1532 MW. Coal is the main fuel. BOT Elektrownia Opole S.A. holds ISO certificate 14001 for Environmental Management Systems, SA certificate 8000 for social responsibility and three certificates for Health and safety (OHSAS 18001; PN-N 18001; level 7 of the International Safety Rating System ISRS, pursuant to the OES area examination techniques).


The situation and the Grundfos solution
The CIM/CIU 150 is a standard interface for data transmission between Profibus DP network and a Grundfos pump or controller. It makes data exchange possible between Grundfos pumping systems and a PLC or SCADA system.

BOT Elektrownia Opole S.A. power plant has an existing installation of several Grundfos CRNE multistage pumps (delivering solution water and urea which is sprayed through nozzles into the power plant's chimney).
The current system contains:

  • 10 CRNE 1-23 (product no. 96570982)
  • 2 CRNE 5-29 (product no. 96518538)

In the power plant these pumps should be controlled by the main process control system Teleperm (Siemens). The complete pump system was delivered and installed by an external Swedish company using a local Polish contractor. The existing data transmission used Profibus protocol, but the existing system was delivered without CIM/CIU modules.

Grundfos Poland offered the prefect solution: Grundfos CIM/CIU. For Grundfos CIM/CIU 150 modules no custom programming is needed to integrate them in a Profibus network. The system integration is very straight-forward. Now the new add-on-equipment includes Grundfos CIU modules and a Siemens PLC system, which provides full control of pumps and S7 300.


The outcome

BOT Elektrownia Opole S.A. power plant is very satisfied because all Grundfos pumps and the new control solution have performed very well. Now local technicians can control and monitor all connected pumps via CIM 150. And these pumps are very critical ones: If they stop running and the NOx concentration reaches a too high level the control system will immediately stop the complete power block.

Chủ đề:

The most modern hard coal fuelled power station in Poland relies on the Grundfos CIU 150 – the perfect communication interface for Profibus

Địa điểm:

Poland

Công ty:

BOT Elektrownia Opole S.A. power plant

Advantages at a glance

  • Support wide range of Grundfos products
  • Supports standard intelligent pump profile from Profibus International
  • Modular design - prepared for future needs
  • 24-240 VAC/VDC power supply in CIU
  • Easy installation and commissioning

 

CRNE pumps
All CRNE pumps are connected by Grundfos CIU 150 Profibus to S7 300 PLC and further by Profibus to the central control system Siemens Teleperm. The Polish Grundfos service partner Z.Z.A.M. Janiszewski made transmission software between pumps and S7 300 PLC and installed all devices. These 12 CRNE pumps deliver solution water and urea which is then sprayed through nozzles into the power plant's chimney.
CIU

Supported products

  • Dry-running E-pumps: CRE/CRNE/CRIE, MTRE, CME, TPE series 1000/2000, NBE/NKE
  • CUE motor drive for pumps
  • Multi Pump Controller: Control MPC*
  • Boosters: Hydro Multi-E and Hydro MPC*

 

* Additional add-on GENIbus module required