New life to an old Hotel

Overview_TEXT

Tổng quan

Vilnius, Lithuania: The freshly renovated 22-story Reval Hotel Lietuva offers a warm welcome to international guests travelling either on business, conference or leisure purposes. The hotel is situated on the bank of the River Neris in the centre of Vilnius, only a 10-minute walk from the medieval old town. Many rooms in the hotel have a wonderful view over the old town and River Neris. When the hotel management decided to renovate the hotel, Grundfos was the natural choice as overall pump supplier.


The Situation
As a high-class hotel with multiple uses the Reval Hotel required a complex infrastructure featuring highly durable, high-performance products – with maximum reliability and a minimum of service and maintenance needs. So the hotel management decided to renovate with first-class materials and products. To help plan a successful renovation, Grundfos was selected as expert product supplier. Besides the simple need for change, the motivation was practical. Away with puddles in the basement and water-stains on the ceiling.


The Grundfos Solution
In the heating installation of the building a range of LP pumps were installed as well as Hydro 2000 booster units. The installation furthermore included Grundfos In-line pumps, a range of pumps that provided the hotel with a dramatic reduction in the total life cycle costs of their installations. Furthermore it meant lower energy costs, lower maintenance and service costs, and higher reliability. Put shortly the overall installation reduced total costs considerably. Grundfos supplied all pumps for heating, ventilation, air-conditioning and hot/cold water.


The Outcome

The maintenancestaff of the Reval Hotel is provided with a reliable and efficient system. At the same time the hotel enjoys an economically agreeable, environmentally-friendly and dependable pump system,all to the advantage of hotel guest.

Chủ đề:

Overall solutions - High pumping capacity to meetcustomer expectations - A stable partnership - High reliability at low cost - Grundfos was the natural choice as overall pump supplier.

Địa điểm:

Vilnius, Lithuania

Công ty:

Grundfos

GRUNDFOS PROVIDED

  • Overall solutions
  • High pumping capacity to meetcustomer expectations
  • A stable partnership
  • High reliability at low cost
  • Grundfos was the natural choice as overall pump supplier.

 

Grundfos TP series of In-Line pumps
The new Grundfos TP series of In-Line pumps has been carefully rethought and optimised right across the board.

PROJECT DATA

CHI series
CHI series -a compact and flexible pump solution for a wide range of industrial applications.

PRODUCT DATA

  • Selected Grundfos pumps used:
  • UPS series 100, 200
  • LPDE
  • TP
  • NB/NK
  • CH/CHI
  • CDM
  • Hydro 2000

 

TESTIMONIALS

Grundfos NB
Grundfos NB close and NK long-coupled pumps are ideally suited for use in for instance air-conditioning and heating systems.