RC Pump: Grace under pressure in CO2 refrigeration system

Overview_TEXT

Tổng quan

The world’s first pump optimised for the circulation of liquid CO2 refrigerant is saving money and hassle at a Danish pasta factory, proving its worth to the system supplier, Johnson Controls.

The Grundfos RC pump uses about a third of the energy of the standard, centrifugal pumps that Johnson Controls’ Alexander Cohr Pachai has otherwise used in his decade-long development of the “cascade” refrigeration system. A modern cascade system circulates a natural refrigerant like carbon dioxide (CO2) to all the evaporators in the low-stage part. Another natural refrigerant like propane is used in the upper-stage part to transfer the heat from the low-stage part to the ambient.

Pachai and Grundfos Product Manager Bjarne Dindler Rasmussen first tested RC pumps in a cascade system for a Danish supermarket in 2007. “These pumps turned out to be very efficient compared to the old ones,” says Pachai. In the pasta factory, the old, cast-iron pumps used 3.6 kW of electricity to run, where the stainless steel RC pump needs only 1.3 kW – using 20,000 kWh less over one year. That’s a 64% energy savings. “The energy consumption really surprised me,” Pachai says. “It was so much lower and the pump is very efficient. We see a lot of potential with this new technology.”

A cascade system

Since 2000, Pachai has installed several cascade systems around Scandinavia, the UK and New Zealand. “When I started out, they were first of their kind,” says Pachai, Business Development Manager at global buildings market supplier Johnson Controls. “Now they have become commonplace, and we are producing them in large-scale industrial systems.”

Demand for refrigeration systems using natural refrigerants is rising as legislation and consumers have pressured companies to use natural refrigerants instead of synthetic ones, he says. Natural refrigerants such as CO2 and ammonia (NH3) can significantly reduce the overall environmental impact of refrigeration systems.

How it works

Pachai shows off the CO2/propane cascade system in the engine room at Pastella, a Danish pasta maker owned by Beauvais. “In this case we are refrigerating both the cold stores and the production areas. It’s built on a system where we are pumping CO2 using the Grundfos pumps,” Pachai says. “You pump it out as a liquid,  and then you evaporate parts of this CO2 to generate the refrigerating effect.” The mixture of gas and liquid returns to the vessel, where a pipe takes the gaseous  CO2 to two, compact propane units on the roof of the building. The propane chills the gas through plate heat exchangers, causing it to condense and drip back to  the vessel, where the whole trip begins again, says Pachai.

“I can talk about this system for days, because it is my baby,” he says with a laugh.

No cavitation

In addition to the RC’s energy-saving abilities, Pachai says that it handles the special requirements of CO2 much better than standard centrifugal pumps. Those cannot handle the vapour bubbles that occur when the CO2 liquid accelerates through the rotating impeller. The associated drop in static pressure can cause the CO2 to boil, forming vapour bubbles. These bubbles can cause an immediate reduction in the performance of the pump.

“You lose your cooling capacity when this happens,” Pachai says. “It’s why we always used an additional impeller with the old type, just to overcome this problem. But with this new [RC] pump, there are so many impellers, they are more robust to handling this situation without loss of capacity.”

Rasmussen explains that Grundfos has designed the RC with more impellers than the competitor pumps.

“The RC pumps treat the liquid more gently,” Rasmussen says. “We don’t have to accelerate the liquid as much in the first stage, as is the case for our competitors with fewer stages. This causes less boiling – and therefore fewer problems with loss of performance due to vapour bubbles.”

With its low-required NPSH, the RC does not need the traditional loss-generating protective devices. Designers can thus reduce the dimensions and cost of a system, he adds.

“We anticipate that this pump – designed and optimised for CO2 – will help to increase the efficiency of refrigeration systems and speed up and help the use of CO2 in general,” says Rasmussen.





    Facebook Twitter LinkedIn Technorati

Chủ đề:

The world’s first pump optimised for the circulation of liquid CO2 refrigerant is saving money and hassle at a Danish pasta factory, proving its worth to the system supplier, Johnson Controls.

Địa điểm:

Pastella (Beauvais A/S), Skovlund, Denmark

Công ty:

Johnson Controls