Từ điển bách khoa tìm kiếm

Hiển thị 71 tới 80 của 354 kết quả
Constant pressure, control mode
Constant pressure, control mode
Consumption profile
The consumption profile shows the relationship between the time of the day and the water flow rate.
Control valve
A control valve is used to regulate the amount of a circulating medium to a consuming unit.
Convector
A convector is a heating surface that transfers heat mainly by convection.
Cooling ceiling
Water-carrying cooling ceilings can be used as a supplement, if cooled-air temperature regulation systems are insufficient.
Cooling jacket
A cooling jacket enables a portion of the pumped liquid or an external liquid to be circulated around the motor stator housing.
Cooling surface
A cooling surface is used for cooling of outside air before injection into the building.
Cooling tower
A cooling tower is used to remove excess heat from an air-conditioning system if the heat cannot be utilised for another purpose.
COP (Coefficient of performance)
Coefficient of performance (COP), is an expression of the efficiency of a heat pump.
Corrosion
Corrosion can occur on external and internal surfaces of pipes, tanks and radiators.