Từ điển bách khoa tìm kiếm

Hiển thị 81 tới 90 của 354 kết quả
Corrosion fatigue
Corrosion fatigue describes a situation where a metal is exposed to both mechanical fatigue and corrosion simultaneously.
COSP (Coefficient of system performance)
The COSP of a heat pump is based on the total heat extracted (also referred to as Q) in relation to the energy supplied to the heat pump (also referred to as W).
Crevice corrosion
Generally, metallic corrosion involves the degradation of an exposed metal surface. Corrosion occurs in various forms ranging from uniform attacks over the entire surface to severe local attacks. Crevice corrosion starts more easily than for example pitting corrosion, another form of localized corrosion. Crevice corrosion occurs at narrow openings or spaces between two metal surfaces or between metals and non-metal surfaces. It is usually associated with stagnant conditions in the crevice. ...
Cross flow heat exchanger
A cross-flow heat exchanger exchanges thermal energy from one airstream to another in an air handling unit (AHU).
Decommissioning and disposal costs (Cd)
In the context of life cycle cost, decommissioning and disposal costs are non-existent or modest in commercial building systems.
Decomposition
Decomposition is the breakdown or degradation of complex organic substances into simpler substances by chemical or biological processes.
Degree day
Degree Days are a measure of how cold (or hot) it was over a period of time, and correspondingly how much energy is needed for heating (or cooling) a building.
Detention tank
A detention tank is an artificial flow-control structure that is used to contain stormwater and wastewater for a limited period of a time.
Dew point
The dew point temperature is the temperature where the water content in the air condenses into water.
Diaphragm Tank
Diaphragm tanks are pressurized water vessels where the water and air are separated by a flexible diaphragm allowing the water to expand and absorb pressure surges.