Từ điển bách khoa tìm kiếm

Hiển thị 1 tới 8 của 8 kết quả
Wastewater
Wastewater is a common designation for any water that in one or another way has been affected in quality by human influence.
Water flow rate
Required heating capacity and required temperature differential of the medium are relevant when calculating the design water flow rate for a heating system.
Water hammer
Water hammer can cause pipelines to break or induced damage to equipment if the water hammer is severe enough.
Water hammering
Destructive force that relates to the incompressibility of water.
Water hardness
Hard water can be categorized by the ions found in the water.
Water supply systems in zones
Water supply systems in zones
Water-brine cooled oil cooler
Water-brine cooled oil cooler is an application used to remove a part of the energy input to compress the refrigerant from suction to discharge pressure as well as mechanical friction.
Wet weather flow
Wet weather flow is higher than the dry weather flow due to the contribution from inflow and infiltration in the sewer system.